Drive_Inputs_Level

Drive_Inputs_Level

Address: 8704 (2200H)
Type: WORD
Access:

Read/Write

Unit: --
Range: 0 to 65535
Default Value: 24
Store Supported: Yes
Description:

This register is used to parametrize drive digital inputs working level.

Bit #

Name

Description

Default Value

0

Forward_Limit_Switch_Level

1 = Active high

0 = Active low

0

1

Backward_Limit_Switch_Level

1 = Active high

0 = Active low

0

2

Fast_Stop_Level

1 = Active high

0 = Active low

0

3

Start_Trigger_Level

1 = Active high

0 = Active low

1

4

Stop_Trigger_Level

1 = Active high

0 = Active low

1

5

Reserved

Reserved

0

6

Reserved

Reserved

0

7

Reserved

Reserved

0

8

Reserved

Reserved

0

9

Reserved

Reserved

0

10

Reserved

Reserved

0

11

Start_Trigger_Edge

1 = Input checked on edge

0 = Input checked on level

0

12

Stop_Trigger_Edge

1 = Input checked on edge

0 = Input checked on level

0

13

Reserved

Reserved

0

14

Reserved

Reserved

0

15

Reserved

Reserved

0

Bit Explanation:

 

Forward_Limit_Switch_Level: When this bit is set (1) the drive will consider the forward limit switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close. When this bit is reset (0) the drive will consider the forward limit switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.

 

Backward_Limit_Switch_Level: When this bit is set (1) the drive will consider the backward limit switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close. When this bit is reset (0) the drive will consider the backward limit switch intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.

 

Fast_Stop_Level: When this bit is set (1) the drive will consider the fast stop input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close. When this bit is reset (0) the drive will consider the fast stop input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.

 

Start_Trigger_Level: When this bit is set (1) the drive will consider the start trigger input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close. When this bit is reset (0) the drive will consider the start trigger input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.

 

Stop_Trigger_Level: When this bit is set (1) the drive will consider the stop trigger input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will close. When this bit is reset (0) the drive will consider the stop trigger input intervention when the corresponding digital input (see Drive_Inputs_Setting object) will open.

Notes: --